Everything
 

Print Address Range Settings dialog box


When printing the content of the Disassemble panel, specify an address range of the subject to be printed.

Figure A.35

Print Address Range Settings Dialog Box

 

This section describes the following.

[How to open]

-

On the Disassemble panel, choose [Print...] from the [File] menu.

[Description of each area]

(1)

Range specification area

To specify a range to be printed, select one of the option buttons given below.

(a)

[Current display area] (default)

Prints only a currently displayed range on the Disassemble panel.

(b)

[Current selected area]

Prints only a currently selected range on the Disassemble panel.

However, this is disabled if nothing is selected on the Disassemble panel.

(c)

[Range of specified]

Specify an address range of the subject to be printed by [Start address] and [End address].

Enter an address expression directly in the respective text boxes (specifiable in up to 1,024 characters) or select an input history item from the drop-down list (up to 10 history entries).

Remark

By pressing the [Ctrl] + [Space] keys in this text box, it is possible to complement a symbol name at the current caret position (see "2.21.2 Symbol name completion function").

[Function buttons]

Button

Function

OK

Closes this dialog box and opens a Windows printing dialog box to print a specified range of contents of the Disassemble panel.

Cancel

Closes this dialog box ignoring range selection settings.

Help

Displays help for this dialog box.