Everything
2.2.1 Confirm the connection to a host machine

Connection examples for each debug tool are shown.

Note that the relationship between the microcontroller selected in the project and the connectable debug tools is as the following table.

Remark

"(Serial)"/"(JTAG)" in the table below means that E1/E20 is used with FINE communications or JTAG communications.

Table 2.1

Relationship between Types of Microcontroller and Connectable Debug Tools

Microcontroller

Debug Tool

E1(Serial)

E1(JTAG)

E20(Serial)

E20(JTAG)

EZ Emulator

Simulator

RX610, RX621, RX62N, RX62T, and RX62G Groups

-

 

-

 

-

 

RX630, RX631, RX63N, and RX634 Groups

 

 

 

 

-

 

RX63T Group

 

 

 

 

 

 

RX110, RX111, RX113, RX210, and RX220 Groups

 

-

 

-

 

 

RX21A, RX211, RX231, RX23W, RX23T, RX24T, RX24U, RX130, RX13T and RX23E-A Groups

 

-

 

-

-

 

RX71M, RX66x, RX64M, RX65N, RX651, RX65N-2M, RX651-2M, RX72T, RX72M and RX72N Groups

 

 

 

 

-

 

 

2.2.1.1 [E1]

2.2.1.2 [E20]

2.2.1.3 [EZ Emulator]

2.2.1.4 [Simulator]