2.5.2.1
Changing the download conditions for load module files
To change the download conditions for load module files (whether to load object information or symbol information) under which they are downloaded, follow the procedure described below as you fill in the Download Files dialog box.
(1) | Selection of a load module file |
In the [Download file list] area, select the load module file to download.
(2) | Alteration of download conditions |
In the [Download file list] area, you'll see the download conditions for the currently selected load module file displayed in it.
For each displayed item, change their setting.
|
Download object
|
Specify whether or not to download object information from a specified file.
|
|
Default
|
Yes
|
|
Method to change
|
By selecting from drop-down list
|
|
Specifiable value
|
Yes
|
Downloads object information.
|
|
No
|
Does not download object information.
|
|
Download symbol information
|
Specify whether or not to download symbol information from a specified fileNote 1.
|
|
Default
|
Yes
|
|
Method to change
|
By selecting from drop-down list
|
|
Specifiable value
|
Yes
|
Downloads symbol information.
|
|
No
|
Does not download symbol information.
|
|
Specify the PIC/PID offset
|
Specify whether or not to change the positions of PIC (Position Independent Code) and PID (Position Independent Data) areas of the load module to be downloaded from those at which they were when the load module was created. When this item is changed to [Yes], "PIC Offset" and "PID Offset" are displayed in the sub-item.
|
|
Default
|
No
|
|
Method to change
|
By selecting from drop-down list
|
|
Specifiable value
|
Yes
|
Specifies PIC/PID offsetNote 2.
|
|
No
|
Does not specify PIC/PID offset.
|
|
PIC Offset
|
Enter an offset value from an address that was in the load module when it was created.
For example, if the program section's start address begins with the address 0x1000, enter "1000" for this item. The subject section is downloaded to the address 0x2000.
|
|
Default
|
0
|
|
Method to change
|
By entering directly from the keyboard
|
|
Specifiable value
|
Hexadecimal number in the range 0x0 to 0xFFFFFFFF
|
|
PID Offset
|
Enter an offset value to be set in the PID register that was specified in the load module when it was created.
For example, to set 0x200 in the PID register when the load module is executed, enter "200" for this item.
|
|
Default
|
0
|
|
Method to change
|
By entering directly from the keyboard
|
|
Specifiable value
|
Hexadecimal number in the range 0x0 to 0xFFFFFFFF
|
|
Generate the information for input completion
|
This item is displayed only when the files to be downloaded are in the load-module format.
Specify whether or not to generate information for use by the auto-complete feature while symbol information is being downloaded from a specified file.
If you use the symbol name completion function in "Watch panel", "Memory panel", select is "Yes".
Download time is long in order to generate this information during the download.
|
|
Default
|
Yes
|
|
How to change
|
Select from the drop-down list.
|
|
Specifiable value
|
Yes
|
Generate information for use by the auto-complete feature
|
|
No
|
Does not generate information for use by the auto-complete feature
|
Note 1. | Unless symbol information is downloaded, source-level debugging cannot be performed. |
Note 2. | If you select [Yes] for load modules created not using the PIC/PID functions (see Section “2.7 Usage of PIC/PID Function“), debug operation cannot be guaranteed. |
(3) | Clicking the [OK] button |
Settings you've made in this dialog box are enabled, with the download conditions changed.