This dialog box is used to display the position where a bookmark is to be set or to delete a bookmark.
Figure A.15  | Bookmarks Dialog Box  | 
 
 
The following items are explained here. 
[How to open]
-  | Click the  
 button on the bookmark toolbar.  | 
 
-  | From the [Edit] menu, select [Bookmark] >> [List Bookmarks...].  | 
 
-  | On the Editor panel, select [Bookmark] >> [List Bookmarks...] from the context menu.  | 
 
[Description of each area]
This area displays a list of bookmarks that have been registered.
The bookmarks are listed alphabetically by file name for [Bookmark].  Bookmarks in the same file are listed in line number order.
When a bookmark is added to the Editor panel, a bookmark function is added.
In the bookmark list area, double-clicking on a line moves a caret to the corresponding position for the bookmark.
Displays the name of the file (without any path) in which a bookmark is registered.
Displays the number of the line to which the bookmark is registered.
Displays the path of the file in which the bookmark is registered.
| 
 
View 
 | 
 
Moves a caret to the selected position for the bookmark. 
However, this button is disabled when no bookmark is selected, two or more bookmarks are selected, or no bookmark is registered. 
 | 
| 
 
Remove 
 | 
 
Removes a selected bookmark.  When two or more bookmarks are selected, all of those selected are removed. 
However, this button is disabled when no bookmark is selected or no bookmark is registered. 
 | 
| 
 
Remove All 
 | 
 
Removes all the registered bookmarks. 
This button is disabled when no bookmark is registered. 
 | 
 
Caution  | Registered bookmarks are not deleted even if the Editor panel is closed. 
Note, however, that if the Editor panel in which a file that has never been saved is being displayed is closed, then registered bookmarks will be deleted.  | 
 
[Function buttons]
| 
 | 
 | 
| 
 
Previous 
 | 
 
Moves a caret to the position of the bookmark previous to the selected bookmark. 
This button is disabled in the following cases. 
-  | A bookmark shown in the first line has been selected.  |  
  
-  | No bookmark is selected.  |  
  
-  | Two or more bookmarks are selected.  |  
  
-  | No bookmark is registered.  |  
  
-  | Only one bookmark is registered.  |  
  
 | 
| 
 
Next 
 | 
 
Moves a caret to the position of the bookmark next to the selected bookmark. 
This button is disabled in the following cases. 
-  | A bookmark shown in the last line has been selected.  |  
  
-  | No bookmark is selected.  |  
  
-  | Two or more bookmarks are selected.  |  
  
-  | No bookmark is registered.  |  
  
-  | Only one bookmark is registered.  |  
  
 | 
| 
 
Close 
 | 
 
Closes this dialog box. 
 | 
| 
 
Help 
 | 
 
Displays the help for this dialog box. 
 |