This dialog box is used to find and replace the designated characters.
The   | 
The following items are explained here.
Find/replace is switched when a tab is selected.
This dialog box has the following tabs.
Detailed criteria for searching/replacing is set.
Please see the description of the relevant tabs for details of the contents/how to set.
Buttons for execute find/replace.
Please see the description of the relevant buttons for details.
 button in [Search text] will be displayed only if this dialog box is opened from the