This tab displays information (Product Information) on the [Device List View] selected in the Project Tree panel.
![](r20ut3105ej0110_cscgpv-12.gif)
The following items are explained here.
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View], and then select [Property] from the [View] menu. |
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View], and then select [Property] from the context menu. |
If this panel is already open, selecting a different [Device List View] in the Project Tree panel changes the content displayed accordingly. |
This area displays product information (Release date and Version) on Code Generator.