Everything
2.1 Overview

The CcnvCA78K0R converts extended language specifications (such as macro names, reserved words, #pragma directives, and extended functions) in C source programs for the CA78K0R into extended language specifications for the CC-RL. Then the CcnvCA78K0R generates C source files for the CC-RL.

 

Figure 2.1

Processing Flow in CcnvCA78K0R