The CcnvCA78K0R outputs the conversion result to the standard output. The output format is as follows.
When the -l option is specified, the above output is repeated for the number of files in the list file.
"Message" is output when there is an error or warning. For the output format of a message, see "MESSAGES". When the -r option is specified, the message is output not to the standard output file but to the specified file.
"Input file name" is the input file specified on the command line or in the list file.
"Result" displays any one of the following.
"Number of messages" indicates how many messages were output by message type.