Sets the analog voltage output to the ANOn pin.
[Syntax]
#include "r_cg_macrodriver.h"
void R_12DAn_Set_ConversionValue ( uint16_t reg_value );
Remark n is the channel number.
[Argument(s)]
I/O |
Argument |
Description |
I |
uint16_t reg_value; |
D/A conversion value. |
[Return value]
None.