12-bit D/A converter
Below is a list of API functions output by the Code Generator for 12-bit D/A converter use.
Table 3.50 API Functions: [12-bit D/A Converter]
API Function Name |
Function |
Performs initialization necessary to control the 12-bit D/A converter. | |
Performs user-defined initialization relating to the 12-bit D/A converter. | |
Starts D/A conversion. | |
Ends D/A conversion. | |
Sets the analog voltage output to the ANOn pin. | |
Halts the clock supplied to the 12-bit D/A converter. |