Performs processing in response to the DMA transfer end interrupt INTDMAn.
Remark This API function is called as the interrupt process corresponding to the DMA transfer end interrupt INTDMAn.
[Syntax]
CA78K0R Compiler
__interrupt static void r_dmacn_interrupt ( void );
CC-RL Compiler
static void __near r_dmacn_interrupt ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.