DMA controller
Below is a list of API functions output by the Code Generator for DMA controller use.
Table 3.37 API Functions: [DMA Controller]
API Function Name |
Function |
Performs initialization necessary to control the DMA controller. | |
Performs user-defined initialization relating to the DMA controller. | |
Performs initialization necessary to control the DMA controller. | |
Performs user-defined initialization relating to the DMA controller. | |
Performs processing in response to the DMA transfer end interrupt INTDMAn. | |
Enables operation of channel n. | |
Disables operation of channel n. | |
Starts DMA transfer. |