Writes the data to Data Flash Memories.
[Syntax]
pfdl_status_t R_FDL_Write ( pfdl_u16 index, __near pfdl_u08 * buffer, pfdl_u16 bytecount );
[Argument(s)]
I/O |
Argument |
Description |
I |
pfdl_u16 index; |
Writing start address of Data Flash Memories |
I |
pfdl_u08 * buffer; |
Pointer to a buffer to store the write data |
I |
pfdl_u16 bytecount; |
Total amount of data to wire |
[Return value]
マクロ |
Description |
PFDL_OK |
Normal completion |
PFDL_BUSY |
During execution of the other commands |
PFDL_ERR_WRITE |
Error of the writing |
PFDL_ERR_PARAMETER |
Error of the parameters |