Everything

Data flash libraries

Below is a list of API functions output by the Code Generator for data flash libraries use.

 

Table 3.57   API Functions: [Data Flash Libraries]

API Function Name

Function

R_FDL_Create

Performs initialization necessary to control the Data Flash Libraries.

R_FDL_Open

Starts the Data Flash Libraries.

R_FDL_Close

Stop the Data Flash Libraries.

R_FDL_Write

Writes the data to Data Flash Memories.

R_FDL_Read

Reads the data from Data Flash Memories.

R_FDL_Erase

Erases data for Data Flash Memories.