Everything

r_it_interrupt

Performs processing in response to the 12-bit interval timer interrupt INTIT.

Remark         This API function is called as the interrupt process corresponding to the 12-bit interval timer interrupt INTIT.

 

[Syntax]

CA78K0R Compiler

__interrupt static void   r_it_interrupt ( void );

 

CC-RL Compiler

static void   __near r_it_interrupt ( void );

 

[Argument(s)]

None.

 

[Return value]

None.