Everything

12-bit interval timer

Below is a list of API functions output by the Code Generator for 12-bit interval timer use.

 

Table 3.16 API Functions: [12-Bit Interval Timer]

API Function Name

Function

R_IT_Create

Performs initialization necessary to control the 12-bit interval timer.

R_IT_Create_UserInit

Performs user-defined initialization relating to the 12-bit interval timer.

r_it_interrupt

Performs processing in response to the 12-bit interval timer interrupt INTIT.

R_IT_Start

Starts the count of the 12-bit interval timer.

R_IT_Stop

Ends the count of the 12-bit interval timer.

R_IT_Reset

Reset the 12-bit interval timer.

R_IT_Set_PowerOff

Halts the clock supplied to the 12-bit interval timer.