Halts the clock supplied to the LCD controller/driver.
Remark
1. Calling this API function changes the LCD
controller/driver to reset status.
For this reason, writes to the control
registers after this API function is called are ignored.
Remark
2. This API function stops the clock supply to the
LCD controller/driver, by operating the RTCEN bit of peripheral enable register
n.
For this reason, this API function also stops the clock supply to
other peripheral devices sharing the RTCEN bit (e.g. real-time
clock).
[Syntax]
void R_LCD_Set_PowerOff ( void );
[Argument(s)]
None.
[Return value]
None.