LCD controller/driver
Below is a list of API functions output by the Code Generator for LCD controller/driver use.
Table 3.35 API Functions: [LCD Controller/Driver]
API Function Name |
Function |
Performs initialization necessary to control the LCD controller/driver. | |
Performs user-defined initialization relating to the LCD controller/driver. | |
Performs processing in response to the LCD frame interrupt INTLCD. | |
Sets the LCD controller/driver to display on status. | |
Sets the LCD controller/driver to display off status. | |
Enables operation of internal voltage boost circuit and capacitor split circuit. | |
Disables operation of internal voltage boost circuit and capacitor split circuit. | |
Halts the clock supplied to the LCD controller/driver. | |
Enables operation of internal voltage boost circuit and capacitor split circuit. | |
Disables operation of internal voltage boost circuit and capacitor split circuit. |