Everything

R_PGA_DSAD_Get_AverageResult

Reads the average results of A/D conversion.(mean value)

 

[Syntax]

#include  “r_cg_macrodriver.h”

void       R_PGA_DSAD_Get_AverageResult ( uint16_t * const bufferH, uint16_t * const bufferL );

 

[Argument(s)]

I/O

Argument

Description

O

uint16_t * const bufferH;

Pointer to area in which to store read results of A/D conversion

(DSADMVM resister and DSADMVH resister)

O

uint16_t * const bufferLl;

Pointer to area in which to store read results of A/D conversion

(DSADMVC resister and DSADMVL resister)

 

[Return value]

None.