Everything

24-bit DS A/D converter with programmable gain instrumentation amplifier

Below is a list of API functions output by the Code Generator for 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier use.

 

Table 3.21 API Functions: [24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier]

API Function Name

Function

R_PGA_DSAD_Create

Performs initialization necessary to control the 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier.

R_PGA_DSAD_Create_UserInit

Performs user-defined initialization relating to the 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier.

r_pga_dsad_interrupt_conversion

Performs processing in response to the 24-bit ΔΣ A/D conversion end interrupt INTDSAD.

r_pga_dsad_interrupt_scan

Performs processing in response to the 24-bit ΔΣ A/D scan end interrupt INTDSADS.

R_PGA_DSAD_Start

Starts A/D conversion.

R_PGA_DSAD_Stop

Ends A/D conversion.

R_PGA_DSAD_Set_PowerOff

Halts the clock supplied to the 24-bit ΔΣ A/D converter with programmable gain instrumentation amplifier.

R_PGA_DSAD_Get_AverageResult

Reads the results of A/D conversion.(mean value)

R_PGA_DSAD_Get_Result

Reads the results of A/D conversion.

R_PGA_DSAD_CAMP_OffsetTrimming

Connects the configurable amplifier to the 24-bit ΔΣ A/D converter and trims the offset.

r_pga_dsad_conversion_interrupt

Performs processing in response to the 24-bit ΔΣ A/D conversion end interrupt INTDSAD.

r_pga_dsad_scan_interrupt

Performs processing in response to the 24-bit ΔΣ A/D scan end interrupt INTDSADS.