Performs user-defined initialization relating to the 16-bit timer RJn.
Remark This API function is called as the R_TMRJn_Create callback routine.
[Syntax]
void R_TMRJn_Create_UserInit ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.