Everything

Timer RJ

Below is a list of API functions output by the Code Generator for timer RJ use.

 

Table 3.6   API Functions: [Timer RJ]

API Function Name

Function

R_TMR_RJn_Create

Performs initialization necessary to control the 16-bit timer RJn.

R_TMR_RJn_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer RJn.

r_tmr_rjn_interrupt

Performs processing in response to the timer interrupt.

R_TMR_RJn_Start

Starts the count for 16-bit timer RJn.

R_TMR_RJn_Stop

Ends the count for 16-bit timer RJn.

R_TMR_RJn_Set_PowerOff

Halts the clock supplied to the 16-bit timer RJn.

R_TMR_RJn_Get_PulseWidth

Reads the pulse width of the 16-bit timer RJn.

R_TMRJn_Create

Performs initialization necessary to control the 16-bit timer RJn.

R_TMRJn_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer RJn.

r_tmrjn_interrupt

Performs processing in response to the timer interrupt.

R_TMRJn_Start

Starts the count for 16-bit timer RJn.

R_TMRJn_Stop

Ends the count for 16-bit timer RJn.

R_TMRJn_Set_PowerOff

Halts the clock supplied to the 16-bit timer RJn.

R_TMRJn_Get_PulseWidth

Reads the pulse width of the 16-bit timer RJn.