17.5.13 Idle routine information
The number of idle routine information items that can be specified is defined as being within the range of 0 to 1.
Specifies the language used to describe an idle routine.
The keyword that can be specified for idlatr is TA_HLNG or TA_ASM.
The keyword that can be specified for idlatr is TA_HLNG or TA_ASM.
Specifies the start address for an idle routine.
A value from 0x0 to 0xfffffffe (aligned to a 2-byte boundary), or a symbol name, can be specified for idlrtn.
A value from 0x0 to 0xfffffffe (aligned to a 2-byte boundary), or a symbol name, can be specified for idlrtn.