Everything

ref_cyc

iref_cyc

Outline
Reference cyclic handler state.
C format
 ER      ref_cyc (ID cycid, T_RCYC *pk_rcyc);
 ER      iref_cyc (ID cycid, T_RCYC *pk_rcyc);
Parameter(s)
I/O
Parameter
Description
I
 ID      cycid;
ID number of the cyclic handler to be referenced.
O
 T_RCYC  *pk_rcyc;
Pointer to the packet returning the cyclic handler state.

[Cyclic handler state packet: T_RCYC]
 typedef struct  t_rcyc {
     STAT    cycstat;        /*Current state*/
     RELTIM  lefttim;        /*Time left before the next activation*/
     ATR     cycatr;         /*Attribute*/
     RELTIM  cyctim;         /*Activation cycle*/
     RELTIM  cycphs;         /*Activation phase*/
 } T_RCYC;

Explanation
Stores cyclic handler state packet (current state, time left before the next activation, etc.) of the cyclic handler specified by parameter cycid in the area specified by parameter pk_rcyc.
Note For details about the cyclic handler state packet, refer to "15.2.12 Cyclic handler state packet".
Return value
Macro
Value
Description
E_OK
0
Normal completion.
E_ID
-18
Invalid ID number.
- cycid < 0x0
- cycid > Maximum ID number
E_CTX
-25
Context error.
- This service call was issued in the CPU locked state.
E_NOEXS
-42
Non-existent object.
- Specified cyclic handler is not registered.