This option suppresses the output of information messages.
The output of information messages is suppressed.
If message number num is specified, the output of the message with the specified number is suppressed. |
Specify the 4-digit number that is output after the component number (05) and the phase of occurrence (6) as num (for example, specify 0004 for message number M0560004). |
If a number of a warning or error type message is specified, the output of the message is suppressed assuming that -change_message option has changed the specified message to the information type. |