Everything
3.1.1 Structure of the assemble list

The structure and contents of the assemble list are shown below.

Output Information

Description

Assemble list

Location counter value, code, line number, and source program under assembly

Section list

Type, size, and name of section

Command line information

Character string of command line of assembler