Everything
3.1.4 Command line information

The character string of the command line of the assembler is output.

The output example of the command line information is shown below.

Command Line Parameter
a.asm -Xcommon=rh850 -Xprn_path      (1)

Number

Description

(1)

Character string of command line

The character string of the command line specified for the assembler is output.