The structure and contents of the link map are shown below.
Output Information
Description
Header information
Version information of the optimizing linker and time of linkage
Option information
Option strings specified by a command line or subcommand file
Error information
Error message
Entry information
Execution start address
Combined address information
Combined source files, and start and end addresses and size of continuous range data
Address overlap information
Overlapped combine source files, and start and end addresses and size of overlapped range data