Everything
3.3.2 Header information

The version information and the time of linkage are output.

The output example of the header information is shown below.

Renesas Optimizing Linker (VX.XX.XX)            XX-Xxx-XXXX XX:XX:XX    (1)

Number

Description

(1)

Version information of the optimizing linker and time of linkage

The version information of the optimizing linker and the time of linkage are output.