Everything
2.19.7.2 Event types that can be set and deleted during execution

The following types of events can be set or deleted during program execution, or during tracer/timer execution.

Table 2.30

Event Types That Can be Set and Deleted during Execution

Event Type

Debug Tool

Full-spec emulator/E1/E20

GTM

Simulator

Hardware Break
(after execution)

 

NG

-

Hardware Break
(before execution)

 

-

 

Software Break

NG

-

-

Trace (trace start/trace end)

Point Trace

 

-

 

Timer Result
(timer start/timer end)

NG

-

 

Performance Measurement
(performance measurement start/
performance measurement end)

NG

-

-

Action
(Printf)

NG

-

 

 

: Possible, if the program execution is allowed to pause for eventsNote

: Impossible while tracer or timer is executing

: Impossible while tracer or timer is executing. Possible, if the program execution is allowed to pause for eventsNote

NG : Impossible

: Not supported

Note

To enable this, specify [Yes] with the [Set event by stopping execution momentarily] property in the [Set Event While Running] category on the [Debug Tool Settings] tab of the Property panel.