This timer operation can be configured in the [Trace] category on the [Debug Tool Settings] tab in the Property panel.

Select the frequency division ratio of the timer counter (120 MHz) used for timer measurement (default: [1/1(8ns/0.6min)]).
It is not possible to divide the timer counter for the Run-Break time (see "2.12.2 Measure execution time until stop of the execution"). |