Everything
2.8.5 Stop the program with the access to variables/SFRs

By setting a break event with the access, the program can be stopped when an arbitrary variable or SFR is accessed with the specified type.

You can also limit the accessed value.

The following types can be specified with the access.

Table 2.5

Types of Accesses to Variables

Access Type

Description

Read

The program is stopped with the read access to (after reading) the specified variable/SFR.

Write

The program is stopped with the write access to (after writing) the specified variable/SFR.

Read/Write

The program is stopped with the read access/write access to (after reading or writing) the specified variable/SFR.

Caution

[IECUBE][E1][E20][EZ Emulator]
The program is stopped with the access via DMA (Direct Memory Access).

 

This section describes the following.

 

2.8.5.1 Set a break event (access type)

2.8.5.2 Edit a break event (access type)

2.8.5.3 Delete a break event (access type)