Move the caret to a specified position.
This section describes the following.
On the Disassemble panel, select [Go To…] on the context menu.  | 
On the IOR panel, select [Go To…] on the context menu.  | 
Specify a location to which you want the caret to be moved.
Enter directly in the text box (specifiable in up to 1,024 characters) or select an input history item from the drop-down list (up to 10 history entries).
The content of specification differs with the panel concerned, as shown below.
If this dialog box is opened from the Disassemble panel by pressing the [Ctrl] + [Space] keys in the text box here, it is possible to complement a symbol name at the current caret position (see "2.21.2 Symbol name completion function").  |