Everything
 

Trace Search dialog box


This dialog box searches for trace data (see Section "2.13.8 Searching for trace data").

Before performing a search, it is possible to choose whether the search is made at the instruction level or source level.

Figure A.36

Trace Search Dialog Box

 

This section describes the following.

[How to open]

-

Click the toolbar button on the Trace panel.

-

Choose [Find…] from the context menu on the Trace panel.

[Description of each area]

(1)

Tab selection area

Selecting a tab switches the level at which a search is performed.

This dialog box has the following tabs:

(2)

Search condition setting area

Set specific conditions under which a search is performed.

For details about display contents and on how to set, see the section in which the relevant tab is described.

[Function buttons]

Button

Function

Search Backward

Performs a search in the direction toward smaller addresses within a specified range.

The searched spot is put in selected state on the Trace panel.

However, if an invalid value is specified or when the program is under execution, a message is displayed and a search of trace data is not performed.

Also, if the Trace panel is hidden, or if focus is moved to this dialog box while focus was present on another panel, this button is disabled.

Search Forward

Performs a search in the direction toward larger addresses within a specified range.

The searched spot is put in selected state on the Trace panel.

However, if an invalid value is specified or when the program is under execution, a message is displayed and a search of trace data is not performed.

Also, if the Trace panel is hidden, or if focus is moved to this dialog box while focus was present on another panel, this button is disabled.

Cancel

Nullifies the setting for a search of trace data and closes this dialog box.

Help

Displays help for this dialog box.