Everything

A.1 Description

Below is a list of the windows related to tools offered in the real-time OS package.
Table A-1. Window/Panel/Dialog Box List
Window/Panel/Dialog Box Name
Function Description
The first window opened when CS+ starts.
Create Project dialog box
Creates a new project or subproject.
(See "CS+ Start" for details.)
Project Tree panel
Displays the project elements as a tree.
(See "RI78V4 V2.xx.xx/RI850V4 V2.xx.xx/RI600V4/RI600PX/RI850V4/RI850MP/RI78V4 Coding" for details.)
Property panel
Displays details and change the settings of the node selected in the Project Tree panel.
(See "RI78V4 V2.xx.xx/RI850V4 V2.xx.xx/RI600V4/RI600PX/RI850V4/RI850MP/RI78V4 Real-Time Operating System User's Manual: Coding" for details.)
Realtime OS Resource Information panel
Displays real-time OS resource information (system information, memory area information, etc.).
(See "RI78V4 V2.xx.xx/RI850V4 V2.xx.xx/RI600V4/RI600PX/RI850V4/RI850MP/RI78V4 Real-Time Operating System User's Manual: Debug" for details.)
Realtime OS Task Analyzer panel
[RI78V4 V2.xx.xx][RI850V4 V2.xx.xx]
[RI600V4]
Displays information required to analyze the processing program (the status of execution transition of programs being processed, usage of real-time OS resources, usage of the CPU, etc.).
(See "RI78V4 V2.xx.xx/RI850V4 V2.xx.xx/RI600V4 Real-Time Operating System User's Manual: Analysis" for details.)
Program analyzer window (AZ850V4 window) [RI850V4 V1.xx.xx]
Executes basic operation of program analyzer.
(See "RI850V4 Real-Time Operating System User's Manual: Analysis" for details.)
Program analyzer window (AZ78K0R window) [RI78V4 V1.xx.xx]
Executes basic operation of program analyzer.
(See "RI78V4 Real-Time Operating System User's Manual: Analysis" for details.)