Reads the alarm conditions (weekday, hour, minute).
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
void R_RTC_Get_AlarmValue ( rtc_alarm_value_t * const alarm_val );
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       rtc_alarm_value_t * const alarm_val;  | 
    
       Pointer to structure in which to store the conditions being read  | 
Remark See R_RTC_Set_AlarmValue for details about rtc_alarm_value_t (alarm conditions).
[Return value]
None.