Sets the cycle of the interrupts INTRTC, then starts the cyclic interrupt function.
[Syntax]
#include “r_cg_macrodriver.h”
#include “r_cg_rtc.h”
MD_STATUS R_RTC_Set_ConstPeriodInterruptOn ( rtc_int_period_t period );
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
rtc_int_period_t period; |
Interrupt INTRTC cycle HALFSEC: 0.5 seconds ONESEC: 1 second ONEMIN: 1 minute ONEHOUR: 1 hour ONEDAY: 1 day ONEMONTH: 1 month |
[Return value]
|
Macro |
Description |
|
MD_OK |
Normal completion |
|
MD_ARGERROR |
Invalid argument specification |