Starts RSPI transmission.
Remark 1. This API function repeats the byte-level RSPI transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num.
Remark 2. When performing a RSPI transmission, R_RSPIn_Start must be called before this API function is called.
[Syntax]
#include "r_cg_macrodriver.h"
MD_STATUS R_RSPIn_Send ( uint32_t * const tx_buf, uint16_t tx_num );
Remark n is the channel number.
[Argument(s)]
I/O |
Argument |
Description |
I |
uint32_t * const tx_buf; |
Pointer to a buffer storing the transmission data |
I |
uint16_t tx_num; |
Total amount of data to send |
[Return value]
Macro |
Description |
MD_OK |
Normal completion |
MD_ARGERROR |
Invalid argument tx_num specification |