Serial peripheral interface (RSPI)
Below is a list of API functions output by the Code Generator for serial peripheral interface use.
Table 3.28 API Functions: [Serial Peripheral Interface]
API Function Name |
Function |
Performs initialization necessary to control the serial peripheral interface. | |
Performs user-defined initialization relating to the serial peripheral interface. | |
Performs processing in response to the receive buffer full interrupts. | |
Performs processing in response to the transmit buffer error interrupts. | |
Performs processing in response to the RSPI error interrupts. | |
Performs processing in response to the RSPI idle interrupts. | |
Starts RSPI communication. | |
Ends RSPI communication. | |
Starts RSPI transmission. | |
Starts RSPI transmission/reception. | |
Performs processing in response to the receive buffer full interrupts. | |
Performs processing in response to the RSPI error interrupts. | |
Performs processing in response to the RSPI idle interrupts. |