Everything

R_SCIFAn_Serial_Send_Receive

Starts FIFO embedded SCI transmission/reception (clock synchronous mode).

Remark 1.      This API function repeats the byte-level SCI transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num.

Remark 2.      This API function repeats the byte-level SCI reception from the buffer specified in argument rx_buf the number of times specified in argument rx_num.

Remark 3.      When performing a SCI transmission/reception, R_SCIFAn_Start must be called before this API function is called.

 

[Syntax]

#include       "r_cg_macrodriver.h"

MD_STATUS   R_SCIFAn_Serial_Send_Receive ( uint8_t * const tx_buf, uint16_t tx_num,

 uint8_t * const rx_buf, uint16_t rx_num );

Remark         n is the channel number.

 

[Argument(s)]

I/O

Argument

Description

I

uint8_t * const tx_buf;

Pointer to a buffer storing the transmission data

I

uint16_t tx_num;

Total amount of data to send

O

uint8_t * const rx_buf;

Pointer to a buffer to store the reception data

I

uint16_t rx_num;

Total amount of data to receive

 

[Return value]

Macro

Description

MD_OK

Normal completion

MD_ARGERROR

Invalid argument