FIFO embedded serial communications interface (SCIFA)
Below is a list of API functions output by the Code Generator for FIFO embedded serial communications interface use.
Table 3.26 API Functions: [FIFO Embedded Serial Communications Interface]
API Function Name |
Function |
Performs initialization necessary to control the FIFO embedded serial communications interface. | |
Starts FIFO embedded SCI communication. | |
Ends FIFO embedded SCI communication. | |
EStarts FIFO embedded SCI transmission (asynchronous mode). | |
Starts FIFO embedded SCI reception (asynchronous mode). | |
Starts FIFO embedded SCI transmission/reception (clock synchronous mode). | |
Performs user-defined initialization relating to the FIFO embedded serial communications interface. | |
Performs processing in response to the transmit-end interrupts. | |
Performs processing in response to the transmit FIFO data empty interrupts. | |
Performs processing in response to the receive FIFO data full interrupts. | |
Performs processing in response to the framing error or parity error interrupts. | |
Performs processing in response to the break or overrun interrupts. | |
Performs processing in response to the receive data ready interrupts. | |
Performs processing in response to the transmit-end interrupts. | |
Performs processing in response to the receive FIFO data full interrupts. | |
Performs processing in response to the error interrupts. |