Performs processing in response to the receive-data-full interrupts.
Remark This API function is called as the r_scin_receive_interrupt callback routine.
[Syntax]
static void r_scin_callback_receiveend ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.