Everything

Serial communications interface (SCI)

Below is a list of API functions output by the Code Generator for serial communications interface use.

 

Table 3.25 API Functions: [Serial Communications Interface]

API Function Name

Function

R_SCIn_Create

Performs initialization necessary to control the serial communications interface.

R_SCIn_Create_UserInit

Performs user-defined initialization related to the serial communications interface.

r_scin_transmitend_interrupt

Performs processing in response to the transmit-end interrupts.

r_scin_transmit_interrupt

Performs processing in response to the transmit-data-empty interrupts.

r_scin_receive_interrupt

Performs processing in response to the receive-data-full interrupts.

r_scin_receiveerror_interrupt

Performs processing in response to the receive error interrupts.

R_SCIn_Start

Starts SCI communication.

R_SCIn_Stop

Ends SCI communication.

R_SCIn_Serial_Send

Starts SCI transmission (synchronous mode).

R_SCIn_Serial_Receive

Starts SCI reception (synchronous mode).

R_SCIn_Serial_Multiprocessor_Send

Starts SCI transmission (multi-processor communications function).

R_SCIn_Serial_Multiprocessor_Receive

Starts SCI reception (multi-processor communications function).

R_SCIn_Serial_Send_Receive

Starts SCI transmission/reception (clock synchronous mode).

R_SCIn_SmartCard_Send

Starts SCI transmission (smart card interface mode).

R_SCIn_SmartCard_Receive

Starts SCI reception (smart card interface mode).

R_SCIn_IIC_Master_Send

Starts SCI master transmission (simple I2C mode).

R_SCIn_IIC_Master_Receive

Starts SCI master reception (simple I2C mode).

R_SCIn_SPI_Master_Send

Starts SCI master transmission (simple SPI mode).

R_SCIn_SPI_Master_Send_Receive

Starts SCI master transmission/reception (simple SPI mode).

R_SCIn_SPI_Slave_Send

Starts SCI slave transmission (simple SPI mode).

R_SCIn_SPI_Slave_Send_Receive

Starts SCI slave transmission/reception (simple SPI mode).

R_SCIn_IIC_StartCondition

Sends the start bit.

R_SCIn_IIC_StopCondition

Sends the stop bit.

r_scin_callback_transmitend

Performs processing in response to the transmit-end interrupts.

r_scin_callback_receiveend

Performs processing in response to the receive-data-full interrupts.

r_scin_callback_receiveerror

Performs processing in response to the receive error interrupts.