Everything

[RI78V4] tab

Outline
This tab shows the detailed information on the RI78V4 to be used categorized by the following.
- Version Information
Display image
Explanation of each area
1 ) [Version Information]
The detailed information on the version of the RI78V4 are displayed.
Kernel version
Display the version of the RI78V4 to be used.
Note that the version is set permanently when the project is created, and cannot be changed.
Default
Using the RI78V4 version
How to change
Changes not allowed
Install folder
Display the folder in which the RI78V4 to be used is installed with the absolute path.
Default
The folder in which the RI78V4 to be used is installed
How to change
Changes not allowed
Memory model
Display the memory model set in the project.
Display the same value as the value of the [Memory model type] property of the build tool.
Default
The memory model selected in the property of the build tool
How to change
Changes not allowed