This tab displays the alarm handler information (e.g. Alarm Handler Name and ID) of the RI600V4.
 
 Figure A-26.    [Alarm Handler] Tab
 
 The following items are explained here.
 
 -	 From the [Debug] menu, select [Download].
 
 -	 From the [View] menu, select [Realtime OS] >> [Resource Information].
 
 [Description of each area]
 
 (1)	 Information display area
 
 This area displays the alarm handler information (e.g. Alarm Handler Name and ID) of the RI600V4.
 
 This area consists of the following items.
 
 
  
  
    | 
 | 
    
 An icon indicating the current status of the alarm handler and the name of the alarm handler are shown in the following format.
  
 | 
  
  
    | 
 | 
    
 Non-operational state (STP state)
  
 | 
  
  
    | 
 | 
    
 Operational state (STA state)
  
 | 
  
  
    | 
 | 
    
 The ID of the alarm handler is shown.
  
 | 
  
  
    | 
 | 
    
 The current status of the alarm handler is shown.
  
 | 
  
  
    | 
 | 
    
 Non-operational state (STP state)
  
 | 
  
  
    | 
 | 
    
 Operational state (STA state)
  
 | 
  
  
    | 
 | 
    
 The time left before the next activation of the alarm handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
  
 | 
  
  
    | 
 | 
    
 The start address of the alarm  handler is shown.
  
 | 
  
  
    | 
 | 
    
 The extended information of the alarm handler is shown.
  
 | 
  
 
 The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
 
 
  
  
    | 
 | 
    
 Displays cascade menus for selecting the header items to display.
  
 | 
  
  
    | 
 | 
    
 | 
    
 The following items are displayed for selection.
  
 Alarm Handler Name, ID, Status, Time Left, Start Address, Extended Information
  
 | 
  
  
    | 
 | 
    
 The item in question will be displayed.
  
 | 
  
  
    | 
 | 
    
 The item in question will not be displayed.
  
 | 
  
  
    | 
 | 
    
 Displays cascade menus for selecting the display notation.
  
 | 
  
  
    | 
 | 
    
 | 
    
 The following items are displayed for selection.
  
 ID, Time Left, Start Address, Extended Information
  
 | 
  
  
    | 
 | 
    
 Displays value in signed decimal number.
  
 | 
  
  
    | 
 | 
    
 Displays value in hexadecimal number.
  
 | 
  
 
 
  
  
    
 Jump to Source (Start Address)
  
 | 
    
 Opens the Editor panel, and displays the source code of the alarm handler.
  
 | 
  
  
    
 Jump to Disassemble (Start Address)
  
 | 
    
 Opens the Disassemble panel, and displays the results of disassembling the alarm handler.
  
 | 
  
  
    | 
 | 
    
 Resets the item displayed to initial state.
  
 |