| 
 | 
    
 An icon indicating the current status of the cyclic handler and the name of the cyclic handler are shown in the following format.
  
 | 
  
  
    | 
 | 
    
 Non-operational state (STP state)
  
 | 
  
  
    | 
 | 
    
 Operational state (STA state)
  
 | 
  
  
    | 
 | 
    
 The ID of the cyclic handler is shown.
  
 | 
  
  
    | 
 | 
    
 The current status of the cyclic handler is shown.
  
 | 
  
  
    | 
 | 
    
 Non-operational state (STP state)
  
 | 
  
  
    | 
 | 
    
 Operational state (STA state)
  
 | 
  
  
    | 
 | 
    
 The activation cycle of the cyclic handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
  
 | 
  
  
    | 
 | 
    
 The initial activation phase of the cyclic handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
  
 | 
  
  
    | 
 | 
    
 The time left before the next activation of the cyclic handler is shown. A unit of the time is millisecond. But the unit is a basic clock count when a denominator of base clock interval time (tic_deno) is 1.
  
 | 
  
  
    | 
 | 
    
 The start address of the cyclic handler is shown.
  
 | 
  
  
    | 
 | 
    
 The extended information of the cyclic handler is shown.
  
 | 
  
  
    | 
 | 
    
 The attributes of the cyclic handler (initial activation state and existence of saved activation phases) are shown in the following format.
  
 Initial activation state  Existence of saved activation phases
  
 | 
  
  
    
 [Initial activation state of cyclic handler]
  
 | 
  
  
    | 
 | 
    
 Operational state (STA state)
  
 | 
  
  
    | 
 | 
    
 Non-operational state (STP state)
  
 | 
  
  
    
 [Existence of saved activation phases]
  
 | 
  
  
    | 
 | 
    
 There are saved activation phases.
  
 | 
  
  
    | 
 | 
    
 There are no saved activation phases.
  
 |