| Specified Section dialog box | 
This dialog box is used to specify the range for skipping step execution.
| 
Figure A.52 | Specified Section Dialog Box | 
 
This section describes the following. 
[How to open]
[Description of each area]
| 
(1) | [Specified section list] area  | 
This area is used to display the list of the range for skipping step execution.
To add a new section, click the [Add] button in this area, then in the [Specified section property] area, specify the sections to add.
|  |  | 
| 
Up | 
Moves the selected section up one row in the list.  
Clicking this for the top section in the list has no effect. | 
| 
Down  | 
Moves the selected section down one row in the list. 
Clicking this for the bottom section in the list has no effect. | 
| 
Add | 
Adds an empty item "-" to the list, and selects it.   
Specify the section to add in the [Specified section property] area.  | 
| 
Remove | 
Removes the selected section from the list.  | 
| 
(2) | [Specified section property] area | 
This area is used to display or edit the section selected in the [Specified section list] area. 
It can also be used to specify the new sections added via the [Add] button.
| 
Section select type | 
Specify the method for specifying the section. | 
| 
Default | 
Section name | 
| 
Modifying | 
Select from the drop-down list. | 
| 
Available values | 
Section name | 
Specifies the range by the section name. | 
| 
Start and end address | 
Specifies the range by the start and end address. | 
| 
Section name | 
Specify the section name.  
Note that this item appears only when [Section select type] is set to [Section name]. | 
| 
Modifying | 
Directly enter from the keyboard.  | 
| 
Start address | 
Specify the start address.  
Note that this item appears only when [Start and end address] is set to [Section name]. | 
| 
Modifying | 
Directly enter from the keyboard.  | 
| 
End address | 
Specify the end address.  
Note that this item appears only when [Start and end address] is set to [Section name]. | 
| 
Modifying | 
Directly enter from the keyboard.  | 
[Function buttons]
|  |  | 
| 
OK | 
Finishes configuring the target sections, and closes this dialog box.  | 
| 
Cancel | 
Cancels any changes to the target sections, and closes this dialog box.  | 
| 
Help | 
Displays the help for this dialog box.  |