Windows/panels/dialog boxes for debugging are listed below.
| Controls the program execution. Various windows, panels and dialog boxes can be opened from this window. | |
| Selects a core (PE) to be debugged and displays the core status. | |
| Displays detailed information on the debug tool currently selected in the Project Tree panel, and enables the settings of the tool to be changed. | |
| Displays the results of memory value disassemble and is used to execute line assemble and instruction level debug. | |
| Displays the contents of CPU registers, and modifies register values. | |
| Displays detailed information on set events, switches the events between enabled and disabled, or deletes them. | |
| Displays messages output from the build tool/debug tool/plug-ins, or the results of batch searches carried out using the Find and Replace dialog box. | |
| Sets the contexts on the debug target which details are displayed. | |
| Selects files to be downloaded and sets the download conditions. | |
| Specifies the number of view columns of memory values on the Memory panel. | |
| Specifies an offset value for the address display on the Memory panel. | |
| Sets the address range to print the contents of the Disassemble panel. | |
| Displays and modifies the detailed information on an execution-related event. | |
| Displays and modifies the detailed information on an access-related event. | |
| Displays and modifies the detailed information on the point trace event. | |
| Detailed Settings of Timer Measurement dialog box [Full-spec emulator][E1][E20] | Displays and modifies the detailed information on the timer event. | 
| Detailed Settings of Performance Measurement dialog box [Full-spec emulator][E1][E20] | Displays and modifies the detailed information on the Performance Measurement event. | 
| Sets the scroll range for the Memory panel/Disassemble panel. | |
| Saves the settings and other data displayed in the respective windows/panels/dialog boxes or saves upload data. | |
| Displays the functions that access variables in the form of an orthogonal table. | |
| Checks whether exclusive control is correctly performed for a certain variable and makes the settings required for checking. | |
| This panel is central to the functionality of the solution for pseudo-error debugging. | |
| Select Pseudo-Error dialog box [Full-spec emulator][E1][E20] | Selects ECM pseudo-errors displayed in the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20]. | 
| Sets the breakpoints that are to be registered to the Pseudo-Error Debugging panel [Full-spec emulator][E1][E20]. | |
| Debugging CAN Bus Reception Procedures panel [Full-spec emulator][E1][E20] | This panel is central to the functionality of the solution for debugging of CAN bus reception. | 
| RS-CAN Module Setting dialog box [Full-spec emulator][E1][E20] | |
| Receive Channel Setting dialog box [Full-spec emulator][E1][E20] | |
| Transmit Channel Setting dialog box [Full-spec emulator][E1][E20] | |
| Transmit Frame Setting dialog box [Full-spec emulator][E1][E20] | |
| This panel is central to the functionality of the solution for measurement of CAN bus reception processing times. | |
| This dialog box is used to set conditions for measurement in the Measuring CAN Bus Reception Processing Times panel [E2]. |