Everything
2.1 Overview

The procedure starting from the startup of CS+, creating and building projects, and up to saving projects is shown as follows.

(1)

Start CS+

Start CS+ (see "2.2 Start CS+").

(2)

Create or load a project

Create a new project, or load an existing one (see "2.3 Create a Project" and "2.4 Manipulate a Project").

(3)

Set the build tool version

Set the build tool version (see "2.5 Change the Build Tool Version").

(4)

Set build target files

Add or remove build target files and update the dependencies (see "2.6 Set Build Target Files").

(5)

Set build options

Set the options for the build tool.

Remark

See "CS+ Integrated Development Environment User’s Manual: Build Tool Operation" for details about setting build options.

(6)

Run a build

Run a build after making related settings as required (see "2.7 Make Settings for Build Operations" and "2.8 Run a Build").

Remark

If there are any commands you wish to run before or after the build process, on the build tool's Property panel, from the [Common Options] tab, in the [Others] category, set the [Commands executed before build processing] and [Commands executed after build processing] properties.
If there are any commands you wish to run before or after the build process at the file level, you can set them from the [Individual Compile Options] tab (for a C source file) and [Individual Assemble Options] tab (for an assembly source file).

(7)

Save the project

Save the setting contents of the project to the project file (see "2.9 Save the Project File").

 

In addition to the above, the following operations are possible.

-

Changing the window layout (see "2.10 Change the Window Layout")

-

Accelerating the startup time of CS (see "2.11 Accelerate the Startup Time of CS+")

-

Manipulating CS on the command line (see "2.12 Manipulate CS+ on the Command Line")