This section explains operations on a build.
-
Import the build options of other project
Set the link order of files
Change the build order of subprojects
Display a list of build options
Change the build target project
Add a build mode
Change the build mode
Delete a build mode
Set the current build options as the standard for the project